/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file lora_app.h
* @author MCD Application Team
* @brief Header of application of the LRWAN Middleware
******************************************************************************
* @attention
*
*
© Copyright (c) 2020 STMicroelectronics.
* All rights reserved.
*
* This software component is licensed by ST under Ultimate Liberty license
* SLA0044, the "License"; You may not use this file except in compliance with
* the License. You may obtain a copy of the License at:
* www.st.com/SLA0044
*
******************************************************************************
*/
/* USER CODE END Header */
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __LORA_APP_H__
#define __LORA_APP_H__
#ifdef __cplusplus
extern "C" {
#endif
/* Includes ------------------------------------------------------------------*/
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Exported types ------------------------------------------------------------*/
/* USER CODE BEGIN ET */
/* USER CODE END ET */
/* Exported constants --------------------------------------------------------*/
/* LoraWAN application configuration (Mw is configured by lorawan_conf.h) */
#define ACTIVE_REGION LORAMAC_REGION_AS923
/*!
* CAYENNE_LPP is myDevices Application server.
*/
/*#define CAYENNE_LPP*/
/*!
* Defines the application data transmission duty cycle. 10s, value in [ms].
*/
#define APP_TX_DUTYCYCLE 10000
/*!
* LoRaWAN User application port
* @note do not use 224. It is reserved for certification
*/
#define LORAWAN_USER_APP_PORT 2
/*!
* LoRaWAN Switch class application port
* @note do not use 224. It is reserved for certification
*/
#define LORAWAN_SWITCH_CLASS_PORT 3
/*!
* LoRaWAN default endNode class port
*/
#define LORAWAN_DEFAULT_CLASS CLASS_A
/*!
* LoRaWAN default confirm state
*/
#define LORAWAN_DEFAULT_CONFIRMED_MSG_STATE LORAMAC_HANDLER_UNCONFIRMED_MSG
/*!
* LoRaWAN Adaptive Data Rate
* @note Please note that when ADR is enabled the end-device should be static
*/
#define LORAWAN_ADR_STATE LORAMAC_HANDLER_ADR_ON
/*!
* LoRaWAN Default data Rate Data Rate
* @note Please note that LORAWAN_DEFAULT_DATA_RATE is used only when LORAWAN_ADR_STATE is disabled
*/
#define LORAWAN_DEFAULT_DATA_RATE DR_0
/*!
* LoRaWAN default activation type
*/
#define LORAWAN_DEFAULT_ACTIVATION_TYPE ACTIVATION_TYPE_OTAA
/*!
* User application data buffer size
*/
#define LORAWAN_APP_DATA_BUFFER_MAX_SIZE 242
/*!
* Default Unicast ping slots periodicity
*
* \remark periodicity is equal to 2^LORAWAN_DEFAULT_PING_SLOT_PERIODICITY seconds
* example: 2^3 = 8 seconds. The end-device will open an Rx slot every 8 seconds.
*/
#define LORAWAN_DEFAULT_PING_SLOT_PERIODICITY 4
/* USER CODE BEGIN EC */
/* USER CODE END EC */
/* Exported macro ------------------------------------------------------------*/
/* USER CODE BEGIN EM */
/* USER CODE END EM */
/* Exported functions prototypes ---------------------------------------------*/
/**
* @brief Init Lora Application
*/
void LoRaWAN_Init(void);
/* USER CODE BEGIN EFP */
/* USER CODE END EFP */
#ifdef __cplusplus
}
#endif
#endif /*__LORA_APP_H__*/
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/